Quick and Effective tool solution
                    
                    
         Changes from V9.05.00 to V9.06.00 (Jul. 20, 2021)
1. Added CAN information of RH850/F1KM-S2 [E2 emulator]
    CAN reception processing time measurement is available.
                    
                    
         Changes from V9.04.00 to V9.05.00 (Jan. 20, 2021)
1. Extension of the zoom percentage of the [Measuring Current Consumption] panel : Simulator[RL78] and E2 emulator[RL78 and RX]
                    
                    
         Changes from V3.03.00 to V9.04.00 (Jul. 20, 2020)
1. Improvement of search processing of Measuring Current Consumption Panel [RX][RL78][E2 emulator][simulator]
          
                    
                    
         Changes from V3.02.00 to V3.03.00 (Jul. 22, 2019)
1. Improvement of display processing of Measuring Current Consumption Panel [RX][RL78][E2 emulator][simulator]
          
                    
                    
         Changes from V3.01.00 to V3.02.00 (Jan. 21, 2019)
1. Support for CS + for CC V8.01.00
          
                    
                    
         Changes from V3.00.00 to V3.01.00 (Jul. 20, 2018)
1. Improvement of Measuring CAN bus reception processing times feature [RH850][E2 emulator]
    A change has been made so that the settings of the QE can be linked with the Editor of the active project. 
2. Improvement of Measuring current consumption feature [RX][RL78][E2 emulator]
    A change has been made so that the settings of the QE can be linked with the Editor of the active project. 
          
                    
                    
         Changes from V2.00.00 to V3.00.00 (Jan. 22, 2018)
1. Enhanced facility for use in measuring times in CAN bus transfer and current drawn [E2 emulator]
    When rebuilding and downloading are required at the start of measurement, 
    the CPU can be reset according to the setting of [CPU Reset after download] 
    in the [Download] category on the [Download File Settings] tabbed page of 
    the [Property] panel for the debug tool.
          
                    
                    
         Changes from V1.02.00 to V2.00.00 (Jul. 20, 2017)
1. Addition of Measuring CAN bus reception processing times feature [RH850][E2 emulator]
2. Addition of Measuring current consumption feature [RL78][E2 emulator]
Note: The version of installer is V1.03.00. (CSPlus_QE__V10300.exe)
          
                    
                    
         Changes from V1.01.00 to V1.02.00 (Jan. 20, 2017)
1. Improvement of the tool for checking exclusive control [RH850]
    In accordance with the change of the compiler version, 
    a change has been made so that the setting of whether a button to be started is enabled or disabled is automatically reflected.
    Additionally, the tool name has been renamed "Exclusive control checking tool".
2. Change of a message from pseudo-errors debugging [RH850]
    A message displayed when the [Delete] key in the [Breakpoint List] tree is pressed have been changed.
          
                    
                    
         Changes from V1.00.00 to V1.01.00 (Oct. 5, 2016)
1. Checking for exclusive control in simulation [RH850]
    The facility of checking for exclusive control is now also applicable with the simulator.