Emulator Utilities

The product name of CubeSuite+, an integrated development environment from Renesas, 
has been changed to "CS+" from V. 3.00.00, which was released on October 1, 2014.

Changes from V1.05.00 (CS+ for CC) to V1.06.00 (CS+ for CC) (Jul. 21, 2026)

1. The self-checking program for the E2 emulator has been updated.
2. The self-checking program for the E2 emulator Lite has been updated.

Changes from V1.05.00 (CS+ for CA,CX) to V1.06.00 (CS+ for CA,CX) (Jul. 21, 2026)

1. The self-checking program for the E2 emulator Lite has been updated.

Changes from V1.04.00 (CS+ for CC) to V1.05.00 (CS+ for CC) (Jan. 20, 2023)
Changes from V1.03.00 (CS+ for CA,CX) to V1.05.00 (CS+ for CA,CX) (Jan. 20, 2023)

1. Revamped Windows menu
2. Change the folder of the manuals

Changes from V1.03.00 (CS+ for CC) to V1.04.00 (CS+ for CC) (Sep. 29, 2021)

1. The self-checking program for the E2 emulator has been updated.
    Updated the self-checking program version from V1.01.00 to V.1.02.00.

Changes from V1.02.00 (CS+ for CC) to V1.03.00 (CS+ for CC) (Jul. 20, 2020)
Changes from V1.02.00 (CS+ for CA,CX) to V1.03.00 (CS+ for CA,CX) (Jul. 20, 2020)

1. The self-checking program for the E2 emulator Lite has been added.
2. User's manuals for the E2 emulator Lite has been added.

Changes from V1.00.06 to V1.01.00 (CS+ for CA,CX) (Jul. 22, 2019)

1. User's manuals for the E1/E20 emulators have been updated.
2. The V850 JTAG OCD Checker has been removed from Emulator Utilities.
3. The V850 JTAG OCD Checker UM has been removed from Emulator Utilities.

Changes from V1.01.00 (CS+ for CC) to V1.02.00 (CS+ for CC) (Jul. 20, 2017)

1. The self-checking program for the E2 emulator has been updated.
2. User's manuals for the E2 emulator has been updated.

Changes from V1.00.06 to V1.01.00 (CS+ for CC) (Jan. 20, 2017)

1. User's manuals for the E1/E20 emulators have been updated.

Changes from V1.00.05 to V1.00.06 (Apr. 23, 2013)

We have revised the following note.
- The note for debugging RL78 family and 78K0R microcontroller with 
  CubeSuite+ V2.00.00 and E1 emulator.
  
    If the CubeSuite+ Package V2.00.00 is overwritten to a host PC which the
    CubeSuite+ package V1.03.00 including Emulator Utility V1.00.04 has been
    installed, users cannot debug systems designed with MCUs of the RL78
    Family and 78K0R. (Connection to Debug Tool will not be established.)

    The problem is caused by inconsistencies during installation process,
    which have been confirmed in the CubeSuite+ Package V1.03.00 and
    V2.00.00 including the emulator utility V1.00.04 and V1.00.05, respectively.

    The problem does not arise if:
    - Evaluation Software CubeSuite+ V2.00.00 is newly installed.
    - Evaluation Software CubeSuite+ V2.00.00 is overwritten to CubeSuite+ V1.02.01 or earlier.
      However, the problem arises if the emulator utility has been updated
      to V1.00.04 before the installation of CubeSuite+ V2.00.00.

Changes from V1.00.04 to V1.00.05 (Apr. 16, 2013)

1. Changed the name of N-Wire Checker to V850 JTAG OCD Checker        
2. Addition of correspondence to V850E2M core and V850E2S core to the V850 JTAG OCD Checker
3. Addition of correspondence to E1/E20 Emulator to the V850 JTAG OCD Checker

Changes from V1.00.03 to V1.00.04 (Nov. 1, 2012)

The E1, E20 Self-Checking Program has been upgraded from V1.0.0.01 to V.1.01.00
(1) The function has been added to the product to solve the following problem:
     - When the E1 or E20 emulator is connected, the "emulator serial No." is not correctly displayed.
    The problem will not occur by executing this self-checking program once.
(2) The following program has been fixed:
     - Problem that "Debug Assertion Failed!" message occurs when executing the self-checking program on a specific PC.

Changes from V1.00.02 to V1.00.03 (May 21, 2012)

1. Self-check program added
    E1/E20 self-check program for RX family has been added.
2. Updated document
    E1/E20 emulator user's manual has been updated. 

Changes from V1.00.01 to V1.00.02

Supported Devices Increased
    The following MCUs have been added to the support line of the OCD Checker.

- V850E/Sx3-H
     µPD70F3486, µPD70F3487, µPD70F3488, µPD70F3925, µPD70F3926, 
     µPD70F3927, µPD70F3931, µPD70F3932, µPD70F3933, µPD70F3933, 
     µPD70F3935, µPD70F3936, µPD70F3937, µPD70F3938, µPD70F3939
		  
- V850ES/Jx3-L
     µPD70F3792, µPD70F3793, µPD70F3794, µPD70F3795, µPD70F3796, 
     µPD70F3797, µPD70F3798, µPD70F3799, µPD70F3800, µPD70F3801, 
     µPD70F3802, µPD70F3803, µPD70F3804, µPD70F3805, µPD70F3806, 
     µPD70F3807, µPD70F3808, µPD70F3838, µPD70F3839, µPD70F3840, 
     µPD70F3841, µPD70F3842, µPD70F3843, µPD70F3844

- V850ES/Jx3-H
     µPD70F3809, µPD70F3810, µPD70F3811, µPD70F3812, µPD70F3813, 
     µPD70F3814, µPD70F3815, µPD70F3816, µPD70F3817, µPD70F3818, 
     µPD70F3819, µPD70F3820, µPD70F3821, µPD70F3822, µPD70F3823, 
     µPD70F3824, µPD70F3825

- V850ES/Jx3-E
     µPD70F3826, µPD70F3827, µPD70F3828, µPD70F3829, µPD70F3830, 
     µPD70F3831, µPD70F3832, µPD70F3833, µPD70F3834, µPD70F3835, 
     µPD70F3836, µPD70F3837

Changes from V1.00.00 to V1.00.01

N-wire checker has been added.