Integrated Help
          
           
          
          Change from V2.01.02 to V2.02.01 (Jul. 16, 2014)
The following C compilers  have been supported:
     - CC-RX V2.02.00
     - CC-RH V1.01.00
           
          
          Change from V2.01.01 to V2.01.02 (Jan. 31, 2014)
The following C compiler  has been supported:
     - CA78K0R V1.70
          
           
          
          Change from V2.01.00 to V2.01.01 (Nov. 18, 2013)
The following C compiler  has been supported:
    - CC-RX V2.01.00
           
          
          Changes from V2.00.01 to V2.01.00 (Sep. 30, 2013)
The following C compilers  have been supported:
     - CC-RH V1.00.01
     - CX V1.31
           
          
          Change from V2.00.00 to V2.00.01 (Jun. 17, 2013)
The following compiler has been supported:
    - CC-RX V2.00.01
 
            
          
          Change from V1.03.01 to V2.00.00 (Apr. 16, 2013)
Addition of correspondence to CubeSuite+ V2.00.00.
            
          
          Change from V1.03.00 to V1.03.01 (Feb. 1, 2013)
The following compiler has been supported:
    - CA78K0R V1.60
            
          
          Change from V1.02.01 to V1.03.00 (Nov. 1, 2012)
CubeSuite+ V1.03.00 has been supported.
            
          
          Change from V1.02.00 to V1.02.01 (Aug. 1, 2012)
The following compiler has been supported:
    - CA78K0R V1.41
            
          
          Changes from V1.01.00 to V1.02.00
The following compilers have been supported:
     - CC-RX V1.02.01
     - CA78K0R V1.40
 
             
          
          Changes from V1.00.00 to V1.01.00
The following compilers have been supported:
     - CC-RX V1.02.00
     - CA78K0 V1.21
     - CA78K0R V1.30