USB Driver for Renesas E-Series
The product name of CubeSuite+, an integrated development environment from Renesas,
has been changed to "CS+" from V. 3.00.00, which was released on October 1, 2014.
Changes from V100.00 to V101.00
1. CS+V3.00.00 has been supported.
The install folder has been changed to CS+ folder.
This USB Driver for Renesas E-Series V1.01.00 for CS+ has the same functionality as its USB Driver for Renesas E-Series V1.01.00
for CubeSuite+ (posted on our web site before October 1, 2014).
2. The internal processing has been improved.