USB Driver for MCU Tools
(for 64-bit version of Windows OS)
The product name of CubeSuite+, an integrated development environment from Renesas,
has been changed to "CS+" from V. 3.00.00, which was released on October 1, 2014.
Changes from V2.76.01 to V2.77.00 (Jan. 21, 2019)
The USB driver has supported the IE850A.
Changes from V2.76.00 to V2.76.01 (Oct. 20, 2015)
The USB driver has supported the CS+ V3.02.00.
Changes from V2.61.02 to V2.76.00 (Oct. 1, 2014)
The USB driver has supported the CS+ V3.00.00.
Changes from V2.61.01 to V2.61.02 (Nov. 19, 2012)
The following problem (in RENESAS TOOL NEWS document No. 121119/tn1) has been fixed:
If you use the following host OS and USB driver, the IECUBE2, IECUBE, MINICUBE2, and MINICUBE are not recognized correctly
as hardware by the host PC.
Host OS: 64 bit edition of Windows 7, or 64 bit edition of Windows Vista
USB driver: USB Driver x64 for Renesas MCU Tools V2.61.00, or V2.61.01
Changes from V2.50.02 to V2.61.01
An invalid warning when setting up the driver has been eliminated.