The product name of CubeSuite+, an integrated development environment from Renesas, has been changed to "CS+" from V. 3.00.00, which was released on October 1, 2014. The name of the IECUBE full-spec emulator supporting the V850 family of MCUs, has been changed to IE850 on October 1, 2014.
The USB driver has supported the IE850A.
The USB driver has supported the CS+ V3.02.00.