CS+ Utilities
The product name of CubeSuite+, an integrated development environment from Renesas,
has been changed to "CS+" from V. 3.00.00, which was released on October 1, 2014.
Change from V3.06.00 to V3.06.01 (Jan. 20, 2026)
Update Manager has been improved.
Change from V3.05.00 to V3.06.00 (Jul. 22, 2025)
Microsoft Visual C++ Runtime Library (CS+ operating environment) has been modified.
Microsoft .NET Framework (CS+ operating environment) has been modified.
Change from V3.04.00 to V3.05.00 (Jul. 22, 2019)
Microsoft Visual C++ Runtime Library (CS+ operating environment) has been modified.
Before: Microsoft Visual C++ 2010 SP1 Runtime Library
After: Microsoft Visual C++ 2015 Update 3 Runtime Library
Change from V3.03.00 to V3.04.00 (Jul. 20, 2017)
CS+ V6.00.00 has been supported.
Change from V3.02.00 to V3.03.00 (Jan. 20, 2017)
The license manager has been removed from CS+ Utilities.
Install the license manager V2.00.00 and later separately.
Change from V3.01.01 to V3.02.00 (Apr. 20, 2016)
Addition of correspondence to the following license.
- RH850 License Pack 1 Professional Upgrade (CC-RH)
- RX License Pack 2 Professional Upgrade (CC-RX)
- RL78 License Pack 1 Professional Upgrade (CC-RL)
Change from V3.01.00 to V3.01.01 (Oct. 20, 2015)
The license manager has been improved so that the size of data file which is used internally has been suppressed.
Change from V3.00.00 to V3.01.00 (Apr. 20, 2015)
Addition of correspondence to the following license.
- RL78 License Pack 1 Standard (CC-RL)
- RL78 License Pack 1 Professional (CC-RL)
Change from V2.00.01 to V3.00.00 (Oct. 1, 2014)
CS+ has been supported.
Change from V2.00.00 to V2.00.01 (Sep. 30, 2013)
CubeSuite+ common program V2.01.00 has been supported.
Changes from V1.03.00 to V2.00.00 (Apr. 16, 2013)
1. Addition of correspondence to Windows 8.
2. Addition of correspondence to Microsoft .NET Framework 4.
3. Addition of correspondence to the license for CC-RX V2.
Changes from V1.02.00 to V1.03.00 (Nov. 1, 2012)
CubeSuite+ common program V1.03.00 has been supported.
Changes from V1.01.00 to V1.02.00 (May 21, 2012)
CubeSuite+ common program V1.02.00 has been supported.
Changes from V1.00.00 to V1.01.00
License Manager included in the CubeSuite+ Utilities has supported RX family MCUs.