Update information for CubeSuite
Code Generator for 78K0R/Kx3-L
Changes from V1.11 to V2.00
Changes about GUI
GUI was improved.Changes about DMA controller
DMA controller's following API was corrected. (The mistake was found in RAM end address)Changes about Simplified I2C Communication
When simple IIC was used by the receiving mode, the problem that was not able to be received according to the timing of interrupt was corrected.Changes from V1.00 to V1.11
Changes about GUI
GUI was improved.When simplified IICmn was used, it changed so that the "N-ch" check box of a port setting might be checked automatically.