Update information for CubeSuite
Code Generator for 78K0R/Lx3
Changes from V1.00 to V2.00
Changes about GUI
GUI was improved.Changes about DMA controller
DMA controller's following API was corrected. (The mistake was found in RAM end address)Changes about Simplified I2C Communication
When simple IIC was used by the receiving mode, the problem that was not able to be received according to the timing of interrupt was corrected.Changes about LCD controller and driver
The setting of LCD controller/driver's external resistance division method was changed. The following two API is output by default. "VLCON=0" from LCD_VoltageOff() function was deleted.LCD_VoltageOn()
LCD_VoltageOff()