Update information for CubeSuite
Code Generator for 78K0/Kx2-L
Changes from V1.11 to V2.00
Changes about GUI
GUI was improved.
Changes from V1.00 to V1.11
Changes about GUI
Changes about GUI
When serial interface IICA was used, it changed so that the "N-ch" check box of a port setting might be checked automatically.
The item of "Pseudo RRM function setting " was added to the “system”-“On-chip debug setting” tab.
According to operation conditions, the unit of TM51 interval time corrected the defect always set to "us.“
Changes about generated code
The value of option byte 0083 / 1083H OCDONB bit was always set as 0.