Update information for CubeSuite
Parameter Files for 78K0
Changes from V1.05 to V1.06
Addition of parameter files for following microcontrollers.
- 78K0/DE2
UPD78F0836, UPD78F0837, UPD78F0844, UPD78F0845 - 78K0/DF2
UPD78F0838, UPD78F0839, UPD78F0840, UPD78F0841, UPD78F0842, UPD78F0843, UPD78F0846, UPD78F0847, UPD78F0848, UPD78F0849 - UPD78F0730
UPD78F0730 - 78K0/KC2-C
UPD78F0760, UPD78F0761, UPD78F0762 - 78K0/KE2-C
UPD78F0763, UPD78F0764, UPD78F0765
Changes from V1.04 to V1.05
Addition of parameter files for following microcontrollers.
- 78K0/KB2-A
UPD78F0590, UPD78F0591
- 78K0/KC2-A
UPD78F0592, UPD78F0593
Changes from V1.03 to V1.04
Addition of parameter files for following microcontrollers.
- 78K0/FY2-L
UPD78F0854, UPD78F0855, UPD78F0856 - 78K0/FA2-L
UPD78F0857, UPD78F0858, UPD78F0859 - 78K0/FB2-L
UPD78F0864, UPD78F0865
Changes from V1.02 to V1.03
Addition of parameter files for following microcontrollers.
- 78K0/LE3-M
UPD78F8052, UPD78F8053 - 78K0/LG3-M
UPD78F8054, UPD78F8055
Changes from V1.01 to V1.02
Addition of parameter files for following microcontrollers.
- 78K0/KY2-L
UPD78F0550, UPD78F0551, UPD78F0552, UPD78F0555, UPD78F0556, UPD78F0557 - 78K0/KA2-L
UPD78F0560, UPD78F0561, UPD78F0562, UPD78F0565, UPD78F0566, UPD78F0567 - 78K0/KB2-L
UPD78F0571, UPD78F0572, UPD78F0573, UPD78F0576, UPD78F0577, UPD78F0578 - 78K0/KC2-L
UPD78F0581, UPD78F0582, UPD78F0583, UPD78F0586, UPD78F0587, UPD78F0588 - 78K0/IY2
UPD78F0740, UPD78F0741, UPD78F0742, UPD78F0750, UPD78F0751, UPD78F0752 - 78K0/IA2
UPD78F0743, UPD78F0744, UPD78F0753, UPD78F0754 - 78K0/IB2
UPD78F0745, UPD78F0746, UPD78F0755, UPD78F0756
Changes from V1.00 to V1.01
Addition of parameter files for following microcontrollers.
- 78K0/FC2
UPD78F0881A, UPD78F0882A, UPD78F0883A, UPD78F0884A, UPD78F0885A, UPD78F0886A, UPD78F0895A, UPD78F0894A - 78K0/FE2
UPD78F0887A, UPD78F0888A, UPD78F0889A, UPD78F0890A - 78K0/FF2
UPD78F0891A, UPD78F0892A, UPD78F0893A