Update information for CubeSuite
CubeSuite Parameter Files for V850
Changes from V1.06 to V1.07
The following restriction has been fixed.
Microcontroller:
V850ES/JG3:
UPD70F3739, UPD70F3740, UPD70F3741, UPD70F3742
V850ES/JJ3:
UPD70F3743, UPD70F3744, UPD70F3745, UPD70F3746
V850ES/SG3:
UPD70F3333, UPD70F3334, UPD70F3335, UPD70F3336, UPD70F3340, UPD70F3341, UPD70F3342, UPD70F3343, UPD70F3350, UPD70F3351, UPD70F3352, UPD70F3353
V850ES/SJ3:
UPD70F3344, UPD70F3345, UPD70F3346, UPD70F3347, UPD70F3348, UPD70F3354, UPD70F3355, UPD70F3356, UPD70F3357, UPD70F3358, UPD70F3364, UPD70F3365, UPD70F3366, UPD70F3367, UPD70F3368
Restriction:
If the Erase, Blank check, or Set Security command is executed for programming the flash ROM on any MCU involved, a communication error may arise.
However, that when the command was executed normally with no communication error arising, the erasure, blank checking or security setting has been performed correctly.
Changes from V1.04 to V1.06
Addition of parameter files for following microcontrollers.
V850ES/JC3-L:
UPD70F3797, UPD70F3798, UPD70F3799, UPD70F3800, UPD70F3801, UPD70F3802, UPD70F3803, UPD70F3804, UPD70F3838, UPD70F3839
V850ES/JE3-L:
UPD70F3805, UPD70F3806, UPD70F3807, UPD70F3808, UPD70F3840
V850ES/JG3-L:
UPD70F3841, UPD70F3842, UPD70F3843, UPD70F3844
V850ES/JC3-H:
UPD70F3809, UPD70F3810, UPD70F3811, UPD70F3812, UPD70F3813, UPD70F3814, UPD70F3815, UPD70F3816, UPD70F3817, UPD70F3818, UPD70F3819
V850ES/JE3-H:
UPD70F3820, UPD70F3821, UPD70F3822, UPD70F3823, UPD70F3824, UPD70F3825
Changes from V1.03 to V1.04
Addition of parameter files for following microcontrollers.
V850ES/JG3-L:
UPD70F3792, UPD70F3793, UPD70F3794, UPD70F3795, UPD70F3796
Changes from V1.02 to V1.03
Addition of parameter files for following microcontrollers.
V850ES/JH3-E:
UPD70F3778, UPD70F3779, UPD70F3780, UPD70F3781, UPD70F3782, UPD70F3783
V850ES/JJ3-E:
UPD70F3784, UPD70F3785, UPD70F3786
Changes from V1.01 to V1.02
Addition of parameter files for following microcontrollers.
V850ES/FE3:
UPD70F3370A, UPD70F3371
V850ES/FF3:
UPD70F3372, UPD70F3373
V850ES/FG3:
UPD70F3374, UPD70F3375, UPD70F3376A, UPD70F3377A
V850ES/FJ3:
UPD70F3378, UPD70F3379, UPD70F3380, UPD70F3381, UPD70F3382
V850ES/FK3:
UPD70F3383, UPD70F3384, UPD70F3385
Changes from V1.00 to V1.01
Addition of parameter files for following microcontrollers.
V850E/IG4:
UPD70F3913, UPD70F3914, UPD70F3915
V850E/IH4:
UPD70F3916, UPD70F3917, UPD70F3918
V850E/IG4-H:
UPD70F3919, UPD70F3920, UPD70F3921
V850E/IH4-H:
UPD70F3922, UPD70F3923, UPD70F3924
V850E/SJ3-H:
UPD70F3474, UPD70F3475, UPD70F3476, UPD70F3477, UPD70F3478, UPD70F3479, UPD70F3931, UPD70F3932, UPD70F3933, UPD70F3934, UPD70F3935, UPD70F3936, UPD70F3937, UPD70F3938, UPD70F3939
V850E/SK3-H:
UPD70F3480, UPD70F3481, UPD70F3482, UPD70F3486, UPD70F3487, UPD70F3488, UPD70F3925, UPD70F3926, UPD70F3927