Update information for CubeSuite
Simulator for 78K0R/Kx3
Changes from V2.60 to V2.62.
Simulation on CubeSuite V1.40
Supported simulation on CubeSuite V1.40. There is no functional change.
Changes from V2.43 to V2.60.
Supported simulating the flash shield window (FSW) function.
Supported simulating the flash shield window (FSW) function.
Specifications changed when pressing Alt + F4 together in the simulator's GUI window
Specifications changed not to close it by pressing Alt + F4 together in the simulator's GUI window.Changes from V2.42 to V2.43.
Restrictions eliminated
The restriction described below has been eliminated.
- No.1 Restrictions for disconnection of debug tool
-
[Applies to]
When a limited user (a user who is not an Administrator) is logged into Windows and uses the 78K0R/Kx3 Simulator, the following error message may appear when disconnecting from the debug tool.
"Failed to exit debugger" (Error Number: E0210001)
Once this error occurs, no matter how many times the user attempts to disconnect the debug tool, the same error message will appear, and it will not be possible to exit CubeSuite.