Update information for CubeSuite
Simulator for 78K0R/Lx3
Changes from V2.60 to V2.62.
Simulation on CubeSuite V1.40
Supported simulation on CubeSuite V1.40. There is no functional change.
Addition of target devices
Following target devices are added.
µPD78F1510A(80pin), µPD78F1512A(80pin), µPD78F1513A(100pin), µPD78F1515A(100pin),µPD78F1516A(120pin), µPD78F1518A(120pin)