Update information for CubeSuite
Simulator for V850ES/Jx2
Changes from V2.60 to V2.61.
Simulation on CubeSuite V1.40
Supported simulation on CubeSuite V1.40. There is no functional change.
Addition of target devices
Following target devices are added.
µPD70F3797, µPD70F3798, µPD70F3799, µPD70F3800, µPD70F3801, µPD70F3802,
µPD70F3803, µPD70F3804, µPD70F3805, µPD70F3806, µPD70F3807, µPD70F3808,
µPD70F3792, µPD70F3793, µPD70F3794, µPD70F3795, µPD70F3796, µPD70F3809,
µPD70F3810, µPD70F3811, µPD70F3812, µPD70F3813, µPD70F3814, µPD70F3815,
µPD70F3816, µPD70F3817, µPD70F3818, µPD70F3819, µPD70F3820, µPD70F3821,
µPD70F3822, µPD70F3823, µPD70F3824, µPD70F3825
Changes from V2.43 to V2.60.
Specifications changed when pressing Alt + F4 together in the simulator's GUI window
Specifications changed not to close it by pressing Alt + F4 together in the simulator's GUI window.