Update information for CubeSuite
Device Dependent Information for V850ES/Jx3-H, Jx3-U
Changes from V1.00 to 1.01.
Addition of reserved words for the following peripheral I/O register name.
The following Real-TimeOS is now supported.
UFDRQEN (address 0x240000)
Changes from V1.01 to 1.02.
Address information on the IO register was changed as follows
|