Update information for CubeSuite
Device Dependent Information for 78K0/Ix2
Changes from V1.02 to V1.03
Addition of information for the pin configuration tool of following device packages.
- 78K0/Ix2
Changes from V1.01 to V1.02
- SFR is Added
| SFR | Address
| Reset
| R/W
| Note
|
|---|---|---|---|---|
| TX0CR0L | FF84H |
00H |
R/W |
Lower 8-bit of TX0CR0 can be operated. |
| TX0CR1L | FF86H |
00H |
R/W |
Lower 8-bit of TX0CR1 can be operated. |
| TX0CR2L | FF8AH |
00H |
R/W |
Lower 8-bit of TX0CR2 can be operated. |
| TX0CR3L | FF90H |
00H |
R/W |
Lower 8-bit of TX0CR3 can be operated. |
| TX1CR0L | FF9CH |
00H |
R/W |
Lower 8-bit of TX1CR0 can be operated. |
| TX1CR1L | FFB0H |
00H |
R/W |
Lower 8-bit of TX1CR1 can be operated. |
| TX1CR2L | FFB2H |
00H |
R/W |
Lower 8-bit of TX1CR2 can be operated. |
| TX1CR3L | FFB4H |
00H |
R/W |
Lower 8-bit of TX1CR3 can be operated. |
Changes from V1.00 to V1.01.
Additionn of device files for The following devices.
[new devices]
uPD78F0745(32pin), uPD78F0746(32pin), uPD78F0755(32pin), uPD78F0756(32pin)
The access attribute of the ADS register is changed.
The attribute of ADOAS bit6 was chaged from Read/Write to Read
[Apply devices]
uPD78F0740(16pin), uPD78F0741(16pin), uPD78F0742(16pin), uPD78F0743(20pin),
uPD78F0744(20pin), uPD78F0745(30pin), uPD78F0746(30pin)
The access attribute of TMC00 register is changed.
The attribute of TOC001 bit1 was changed from Read/Write to Read
[Apply devices]
uPD78F0740(16pin), uPD78F0741(16pin), uPD78F0742(16pin), uPD78F0750(16pin),
uPD78F0751(16pin), uPD78F0752(16pin), uPD78F0743(20pin), uPD78F0744(20pin),
uPD78F0753(20pin), uPD78F0754(20pin)
The access attribute of the following register is changed
| register | bit possition | Attribute after it changes | Attribute before it changes |
|---|---|---|---|
| TMC51 | bit6 |
Read |
Read/Write |
| TX0CTL1 | bit0, bit1 |
Read |
Read/Write |
| TX0CTL2 | bit4 |
Read |
Read/Write |
| TX0CTL3 | bit4 |
Read |
Read/Write |
| TX0CTL4 | bit6 |
Read |
Read/Write |
| TX1CTL1 | bit4 |
Read |
Read/Write |
| PM2 | bit2 |
Read |
Read/Write |
[Apply devices]
All devices
The bit possition of TX1CTL1 register was changed.
The position of TX1PWMCE bit was changed from bit4 to bit5.
[Apply devices]
All devices