Update information for CubeSuite
Device Dependent Information for 78K0R/Kx3-L
Changes from V1.02 to V1.03
Addtion of device files for the following devices.
UPD78F1027,UPD78F1028,UPD78F1029,UPD78F1030
Changes from V1.01 to V1.02
Addition of information for the pin configuration tool of following device packages.
78K0R/KE3-L 64-pin F1
78K0R/KG3-L 100-pin F1
Changes from V1.00 to V1.01.
Support function(Pin Configurator) for 78K0R/Kx3-L.
Support 78K0R/KF3-L and 78K0R/KG3-L.