Update information for CubeSuite
Device Dependent Information for 78K0R/Ix3
Changes from V1.12 to V1.13
Addition of information for the pin configuration tool.
Changes from V1.11 to V1.12
Support of the CubeSuite V1.20 or later
Changes from V1.10 to V1.11
Addition of information for 1-bit memory manipulation instruction
with the following special function registers (SFR)
All bits of Timer channel stop register 0 (TT0L)Bit4 of Noise filter enable register 2 (NFEN2)*Note