Update information for CubeSuite
Device Dependent Information for 78K0R/Lx3
Changes from V1.02 to V1.03.
Addition of information for the following devices.
- uPD78F1510A
- uPD78F1512A
- uPD78F1513A
- uPD78F1515A
- uPD78F1516A
- uPD78F1518A
Changes from V1.01 to V1.02.
Addition of information for the pin configuration tool of following device packages.
- 78K0R/LG3 100-pin GC
Changes from V1.00 to V1.01.
- Support functions (Pin Configurator) for 78K0R/Kx3-L.
- Addition of the following special function registers (SFR).
Timer input select register 1 (TIS1) : Only 78K0R/LF3 and 78K0R/LG3
- Addition of information for write access of 1-bit memory manipulation instruction with the following special function registers (SFR).
Bit4 and bit5 of Timer input select register 1 (TIS1) : Only 78K0R/LH3