Update information for CubeSuite
Device Dependent Information for 78K0R/Fx3
Changes from V1.01 to V1.10
Addition of the following registers
DSA2, DSA3, DRA2, DRA2L, DRA2H, DRA3, DRA3L, DRA3H, DBC2, DBC2L, DBC2H, DBC3, DBC3L, DBC3H, DMC2, DMC3, DRC2, DRC3, DMAIF2, DMAIF3, DMAMK2, DMAMK3, DMAPR02, DMAPR03, DMAPR12, DMAPR13 → open public.
(affected devices: uPD78F1812, uPD78F1813, uPD78F1814, uPD78F1815, uPD78F1818, uPD78F1819, uPD78F1820)
Changes from V1.00 to V1.01
An initial value of the CKC register was corrected. This initial value only affects when IECUBE used.
Before change : 09h
After change : 01h