Skip to main content

Update information for CubeSuite

Device Dependent Information for 78K0/Lx3-M

Changes from V1.00 to V1.01

The access attribute of the PM2 resister is changed for 78K0/LE3-M.

The attribute of PM2 for 78K0/LE3-M from bit0 until bit6 was changed from Read to Read/Write.


Changes from V1.00 to V1.01

IECUBE is supported.





Back To Top



End of content

Back To Top


Loading...