Update information for CubeSuite
Device Dependent Information V850 List
Changes from V1.07 to V1.08
Addition of the following device information.
V850E2/Fx4
V850E2/Fx4-H
V850E2/Fx4-M
V850E2/Fx4 Gateway
Changes from V1.06 to V1.07
Addition of the following device information.
V850E/Ix4, V850E/Ix4-HChanges from V1.05 to V1.06
Addition of the following device information.
V850E/Sx3-HChanges from V1.04 to V1.05.
Addition of the following device information.
V850ES/Fx3-LChanges from V1.02 to V1.04.
Addition of the following device information.
V850ES/Fx3Changes from V1.01 to V1.02.
Addition of the following device information.
V850E/Sx3-HChanges from V1.00 to V1.01.
Addition of the following device information.
V850ES/Jx3-EV850E/Ix4
V850E/Ix4-H