How to print this page
Download Site the MCU and firmware files for the M30870T-EPB emulation probe
[For using the PC7501 emulator]


Download methods vary according to debugger.

1. When Using M32C PC7501Emulator debugger

1.1 Confirm Debugger Version
Use the following procedure to make sure M32C PC7501 emulator debugger Version 1.03 Release 00 or later is installed on your system.

  1. Confirm the debugger version and firmware type and version by inputting the VER Command in the debugger script window.
    (Ex.) M32C PC7501 Emulator Target 1.03.00.004
        Firmware "M30870F" V.1.00.00 PC7501
  2. If the debugger will not start up, you can use the auto-update utility to confirm the version of the debugger. Select [Display all applications] in the Application Selection Window, and confirm the version of Application “M32C PC7501 Emulator Debugger”.

If you do not have the latest debugger installed, please update it before proceeding.
The latest version can be updated with the auto-update utility.

1.2 Download Files
Download the firmware update program as follows (extract after downloading).

Content
File name
 
Firmware Update Program m30870fw_mcu_file_installer20070801.exe m30870fw_mcu_file_installer20070801.zip
Download
(ZIP, 3.89MB)
Supplementary Documents rej10j0484_m30870tepb_s.pdf
rej10j0951_m30850t2epb_s.pdf
rjj10j0649_m30870tepb_s.pdf
rjj10j1193_m30850t2epb_s.pdf
Note: This download file is for both M30850T2-EPB and M30870T-EPB.

1.3 Install Files
  1. Confirm that the debugger has not been started.

  2. Execute installer “m30870fw_mcu_file_installer20070801.exe” on the host machine has been installed the debugger. Once the process has begun, follow the instructions displayed on your screen to complete the file installation.

1.4 Download Firmware to PC7501
  1. After installing the file, download the firmware to PC7501. For details, see Chapter 2.7 [Downloading Firmware] in the Users Manual.
    If an error occurs, refer to 1.2 and 1.3 for possible causes, and try the process again.
    (Ex.) Firmware File Copy Error:
        ERROR 16221: Can't download firmware
  2. After downloading the firmware to PC7501, confirm the following 2 items, then perform a self-check to make sure the program has completed successfully. For more details, see Chapter 2.8 [Self-Check] in the Users Manual.

    • If the target system is connected, disconnect it.
    • Re-set the switch in the emulation probe to the original factory settings.

1.5 Confirm Update
To confirm that the program was successfully updated, start the debugger and input the VER Command in the Script Window. Make sure the firmware type and version is M30870F V1.00.00. If the debugger won’t start up, check for possible problems in 1.2 to 1.4 and try the process again.

2. When Using Emulator Debugger M3T-PD308F (Discontinued Product) 

2.1 Confirm Debugger Version
Make sure M3T-PD308F V.3.20 Release 1 (discontinued product) is installed on your system.
  1. Confirm the M3T-PD308F version and firmware type and version by inputting the VER Command in the M3T-PD308F script window.
    (Ex.) M32C PC7501 Emulator Target 1.03.00.004
        Firmware "M30870F" V.1.00.00 PC7501
  2. If M3T-PD308F will not start up, you can confirm the version of the debugger in the Release Notes you received when installing M3T-PD308F. The necessary information is included the Release Notes (pdf file) located in the MANUAL folder in the M3T-PD308F file installation directory.

If you do not have V.3.20 Release 1, update the program as indicated in the following Tool News:
http://tool-support.renesas.com/eng/toolnews/n040401/tn7.htm

2.2 Download File
Download the MCU files and firmware file as follows (extract after downloading).
Content File name  
MCU file m30870.mcu MCU file/Fiemware file
m30870t-epb20070801.zip
Download
(ZIP, 1.67MB)
MCU file m30870_ad.mcu
MCU file m30850.mcu
Firmware file m30870f.s (V.1.00.00)
supplementary document rej10j0484_m30870tepb_s.pdf
rrej10j0951_m30850t2epb_s.pdf
rjj10j0649_m30870tepb_s.pdf
rjj10j1193_m30850t2epb_s.pdf
Note: This download file is for both M30850T2-EPB and M30870T-EPB.

2.3 Copy Files
  1. Confirm the following 2 items in preparation for copying the downloaded files.
    • Make sure the debugger is not turned on.
    • Make sure the following files located in the folder of the debugger installation directory are not being used with any other software.

  2. Copy the MCU files and firmware file to the folders indicated below.
    • Copy (overwrite) ”m30850.mcu”, “m30870.mcu “, and “m30870_ad.mcu to the directory (Mcufiles) that contains the MCU files.
    • Copy “m30870f.s” to the directory that contains the emulator debugger execution file (pd308f.exe).

2.4 Download Firmware to PC7501
After copying the files, download the firmware to PC7501. For details, see Chapter 2.7 [Downloading Firmware] in the Users Manual.
If an error occurs, refer to 2.2 and 2.3 for possible causes, and try the process again.
(Ex.) Firmware File Copy Error:
    ERROR 16221: Can't download firmware
2.5 Confrim Update
To confirm that the program was successfully updated, start the debugger and input the VER Command in the Script Window. Make sure the firmware type and version is M30870F V1.00.00. If the debugger won’t start up or the firmware version is not correct, check for possible problems in Sections 2.2 to 2.4 in the Users Manual and try the process again.

3. Notes
  1. Notes on using the M30870T-EPB are included in the supplementary document (attached to the download file) for each product. Always read these notes before using the product.
  2. Before downloading, refer to the August 1, 2007 issue of RENESAS TOOL NEWS for more information: [A Note on Using the Emulation Probes M30850T2-EPB and M30870T-EPB]



Tool News Index