Renesas has prepared specialized solutions for the user's problems in order to solve various problems encountered in development.
Each solution can be easily accessed from the Solution List panel in CS+.
The Solution List panel can be opened by clicking the [Solution List] button on the toolbar.
Buttons representing each solution are displayed on the panel, and hovering the mouse cursor over each button produces an explanation of the solution in the area on the right side of the window.
The panel for each solution is opened by clicking the button.
The following solutions are currently available in CS+.
The exclusive control checking tool checks whether there is any function that accesses variables outside the exclusive control period.
Pseudo-error debugging is a feature for generating pseudo-errors which are difficult to reproduce on the real machine. You can use this feature to check the operation of the reset routine or handlers called in response to errors, or functions to be called from within handlers, and then debug the code.
Debugging of CAN bus reception is a feature for facilitating debugging of the reception procedure of a channel by continuously transmitting CAN bus frames to a desired channel by using the inter-channel communications facility of the RS-CAN.
Smart browser is a feature for listing various documents (user's manuals, technical updates, application notes, and tool news) related to the device selected for the active project and allowing downloading of sample code, if any, that comes with the applicable application notes.
Smart report is a feature for the collective output of quality-related information such as a list of source files, build option settings, information on functions and variables, and coverage rates.
The optimization performance comparison tool is used to measure and compare the ROM size or execution speed for the case in which the build options recommended by the build tool are applied.