Differences with help information provided by the online help system

This page informs differences between information in the online help system and in user's manuals for CS+ or the offline help system

V8.02.00 (2019/7/22)
The following pages are updated.

The following pages are updated for the usage of Arithmetic Unit for Trigonometric Functions.
Compiler (CC-RX) > COMMAND REFERENCE > Options > Compile Options > Optimize Options > -tfu
Compiler (CC-RX) > COMPILER LANGUAGE SPECIFICATIONS > Extended Language Specifications > Macro Names
Compiler (CC-RX) > COMPILER LANGUAGE SPECIFICATIONS > Extended Language Specifications > Intrinsic Functions
Compiler (CC-RX) > LIBRARY FUNCTIONAL SPECIFICATION > Reentrant Library
Compiler (CC-RX) > STARTUP > Startup Program Creation > Coding Example of Initial Setting Routine