Everything
Differences with help information provided by the online help system

This page informs differences between information in the online help system and in user's manuals for CS+ or the offline help system

V8.09.00 (2023/1/20)
Compiler (CC-RX)
The following pages are updated.

The following page is updated for specification changes in -crc option.
Compiler (CC-RX) > COMMAND REFERENCE > Options > Optimizing Linkage Editor (rlink) Options > Output Options > -crc

Notes on using -entry and -optimize options have been added to the foloowing page.
Compiler (CC-RX) > COMMAND REFERENCE > Options > Optimizing Linkage Editor (rlink) Options > Input Options > -entry

The description of the C standard specification have been corrected on the following pages.
Compiler (CC-RX) > COMPILER LANGUAGE SPECIFICATIONS > Basic Language Specifications > Implementation-defined behavior of C90
Compiler (CC-RX) > COMPILER LANGUAGE SPECIFICATIONS > Internal Data Representation and Areas
Compiler (CC-RX) > LIBRARY FUNCTIONAL SPECIFICATION > Library Function > <stdint.h>

The following messages have been added or changed.
E0523049, E0562220, F0520571, F0563115, W0561017
Compiler (CC-RX) > MESSAGES > MESSAGES > Errors
Compiler (CC-RX) > MESSAGES > MESSAGES > Fatal Errors
Compiler (CC-RX) > MESSAGES > MESSAGES > Warnings

The following pages are updated for the usage of Arithmetic Unit for Trigonometric Functions.(20 April 2023 Additional)
Compiler (CC-RX) > COMMAND REFERENCE > Options > Compile Options > Optimize Options > -tfu_version
Compiler (CC-RX) > COMMAND REFERENCE > Options > Compile Options > Optimize Options > -nosave_tfu
Compiler (CC-RX) > COMPILER LANGUAGE SPECIFICATIONS > Extended Language Specifications > Macro Names
Compiler (CC-RX) > COMPILER LANGUAGE SPECIFICATIONS > Extended Language Specifications > Using Extended Specifications
Compiler (CC-RX) > COMPILER LANGUAGE SPECIFICATIONS > Extended Language Specifications > Intrinsic Functions
Compiler (CC-RX) > STARTUP > Startup Program Creation > Coding Example of Initial Setting Routine
Python Console
The links on the following pages have been fixed.
Python Console > Python CONSOLE/Python FUNCTIONS > CS+ Python Function/Class/Property/Event > CS+ Python function (common)