Everything
 

Property panel


In this panel, the detailed information on the node that is selected in the Project Tree panel is displayed categorized. Also, the settings of the selected node can be changed. This also shows the type of the [Generate Code] button clicked in the Code Generator panel and information about the file selected in the Code Generator Preview panel, and changes settings.

Figure A.11

Property Panel

 

The following items are explained here.

[How to open]

-

Select either one of the Project node, Subproject node, Microcontroller node, Design Tool node, Build Tool node, Debug Tool node, Analyze Tool node, file, or Category node in Project Tree panel. Then select [Property] in [View] menu, or in the context menu.

-

On the Code Generator panel, click [Generate Code] button, and then select [Property] from the [View] menu or context menu.

-

On the Code Generator Preview panel, select file, and then select [Property] from the [View] menu or context menu.

Remark

When either one of the Project node, Subproject node, Microcontroller node, Design Tool node, Build Tool node, Debug Tool node, Analyze Tool node, file, or Category node is selected in Project Tree panel while the Property panel is open, the detailed information of the selected node is displayed.

[Description of each area]

(1)

Name for the selected node area and button group

(a)

Name for the selected node area

In this area, the name of the selected node in Project Tree panel is displayed.

This area is left blank when multiple nodes are selected.

(b)

button group

 

 

Locks properties to prevent the property value from being modified by wrong operation of a mouse or a keyboard.

: locks properties.

: unlocks properties.

 

This button is only on the following tabs.

-

Tabs displayed when the Build Tool node is selected

-

Tabs displayed when the C source file, C++ source file [CC-RX], assembly source file [CC-RH][CC-RL], assembler source file [CC-RX][CC-RL], object file [CC-RH][CC-RL], and object module file [CC-RX]

-

Tabs displayed when the library file is selected (except for [File Information] tab)

 

Opens the Find and Replace dialog box with the [Quick Find] tab target.

Property names, property values, and active-help character strings can be found.

 

Collapses the entire currently displayed detailed information display/change area.

 

Expands the entire currently displayed detailed information display/change area.

(2)

Detailed information display/change area

In this area, the detailed information on the node that is selected in the Project Tree panel is displayed categorized in the list. Also, you can directly change the settings of the selected node. The node includes; Project node, Subproject node, Microcontroller node, Design Tool node, Build Tool node, Debug Tool node, Analyze Tool node, file, and Category node.

The mark indicates all the items in the category are expanded. The mark indicates all the items are shrunk. You can expand/shrink the items by clicking these marks or double clicking the category name.

If the mark is displayed, only the hex number is allowed in the text box.

Please see the information on each tab for the details of the display/setting in the category and its contents.

(3)

Property description area

In this area, brief description of the categories and their contents selected in the Detailed information display/change area is shown.

(4)

Tab selection area

Categories for the display of the detailed information are changed when a tab is selected.

In this panel, the following tabs are contained (see the section explaining each tab for the details on the contents of the display or the method of the setting on the tab).

(a)

When the following nodes are selected in the Project Tree panel

Project node

[Project] tab

Subproject node

[Subproject] tab

Microcontroller node

[Microcontroller Information] tab

Configuration Tool for Multi-core node

[Boot Loader] tab [RH850]

Design Tool node

See "CS+ Integrated Development Environment User’s Manual: Pin Configurator / Code Generator Pin View Operation" and "CS+ Integrated Development Environment User’s Manual: Code Generator Peripheral Function Operation" for details about tabs.

Build Tool node
(Except for a debug-dedicated projectNote)

See the "CS+ Integrated Development Environment User’s Manual: Build Tool Operation" for details about tabs.

Build Tool node
(For a Debug-dedicated projectNote)

[Build Options] tab

Debug Tool node

See the "CS+ Integrated Development Environment User’s Manual: Debug Tool" for details about tabs.

Analyze Tool node

See the "CubeSuite+ Integrated Development Environment User’s Manual: Analysis" for details about this tab.

File

[File Information] tab

 

See the "CS+ Integrated Development Environment User’s Manual: Build Tool Operation" for details about the tabs other than the [File Information] tab.

Category node

[Category Information] tab

Note

For details on the debug-dedicated project, see "E. USING AN EXTERNAL BUILD TOOL".

Remark

When more than two components are selected in Project Tree panel, only the tab that is common to all the components is displayed. If the property is modified, that is taken effect to the selected components all of which are common to all.

[Dialog boxes opened from the Property panel]

The following dialog boxes are opened from the Property panel.

-

Character String Input dialog box

See "Character String Input dialog box" for details.

-

Text Edit dialog box

See "Text Edit dialog box" for details.

-

Path Edit dialog box

See "Path Edit dialog box" for details.

[[Edit] menu (Property panel-dedicated items)]

Undo

Undoes any property changes being done.

Cut

Cuts the selected text to the clip board while editing the property.

Copy

Copies the selected text in the property to the clip board.

Paste

Pastes the contents of the clip board to the property while editing the property.

Delete

Deletes the selected text while editing the property.

Select All

Selects all the text in the selected property while editing the property.

Find...

Opens the Find and Replace dialog box with the [Quick Find] tab target.

[[Help] menu (Property panel-dedicated items)]

Open Help for Property Panel

Displays the help of this panel or the currently displayed tab.

[Context menu]

Undo

Undoes any property changes being done.

Cut

Cuts the selected text to the clip board while editing the property.

Copy

Copies the selected text in the property to the clip board.

Paste

Pastes the contents of the clip board to the property while editing the property.

Delete

Deletes the selected text while editing the property.

Select All

Selects all the text in the selected property while editing the property.

Reset to Default

Restores the configuration of the selected item to default of the project default configuration.

For [Individual Compile Options] tab and [Individual Assemble Options] tab, restores to the configuration of the general option.

Reset All to Default

Restores the configuration of the current tab to default of the project default configuration.

For [Individual Compile Options] tab and [Individual Assemble Options] tab, restores to the configuration of the general option.