Everything
 

[Basic Function] tab


This tab is used to set the build tool and debug tool plug-ins to be read in when this product is started.

Caution

We recommend that the check box for the plug-in for the microcontroller that is the target for development is not deselected.
Deselect the check boxes for the build tool and debug tool plug-ins that are for microcontrollers that are not the target for development. For example, if only the plug-in for the build tool is deselected, the file to be downloaded by the debug tool will not be found and an error will occur.

Figure A.55

Plug-in Manager Dialog Box: [Basic Function] Tab

 

The following items are explained here.

[How to open]

-

From the [Tool] menu, select [Plug-in Setting...].

[Description of each area]

(1)

Plug-in list area

This area shows a list of the build tool and debug tool plug-ins installed in this product, in the following format.

Module Name

Shows the plug-in module names.

The plug-ins read in when this product is started are selected with check boxes.

Description

Shows a simple description of the plug-in.

[Function buttons]

Button

Function

OK

Applies all setting and closes this dialog box.

Cancel

Cancels the designated condition and closes the dialog box.

Help

Displays the help of this dialog box.