Renesas Technology, M3T-F160-EXTC, Accessory Guide, 2004.06.15
Accessry Guide
 
 
M3T-F160-EXTC
Extension Cable for FLX160

Function
The M3T-F160-EXTC is an extension cable used between the compact emulator or emulation probe and the converter board. This cable extends the distance between them up to about 200mm. The connection is one to one.

Package Components
  • M3T-F160-EXTC
  • User's manual



Attaching Procedure
Attach the compact emulator or emulation probe to the EMULATOR side of the M3T-F160-EXTC.
Attach the converter board to the TARGET side of the M3T-F160-EXTC.





Usage








©2005 Renesas Technology Corp., All Rights Reserved.