Renesas Technology, OSC-2, Accessory Guide, 2004.06.15
Accessry Guide
 
 
OSC-2
Oscillator Board (Dumping Resistor Mounting Type)

Function
The OSC-2 is a clock oscillator board that is fitted on an emulation pod or a temporary target board, etc. Users can mount the desired oscillation module on its board.













Circuit Diagram


Dimensions
25.0(D)x32.0(W)mm





©2005 Renesas Technology Corp., All Rights Reserved.