Renesas Technology, IC61-1004-051, Accessory Guide, 2004.06.15
Accessry Guide
 
 
IC61-1004-051
100-pin LCC Socket (Manually Soldering Type) Made by Yamaichi Electronics Co., Ltd.

Function
The IC61-1004-051 is an IC socket that can be soldered to a foot pattern for a 100-pin 0.65mm-pitch QFP (100P6S-A) package MCU (manually soldering type).

Application
Using this IC socket, developers can connect a 100-pin 0.65 mm-pitch LCC package MCU or an emulator probe to the foot pattern on a target that is prepared for a 100P6S-A package MCU. The foot pattern's land length needed to fit the IC socket is a little longer than that of the 100P6S-A.

Dimensions
26.7(D)x23.6(W)x6.6(H)mm

Foot Pattern Reference Dimensions
See Reference Dimensional Drawings for Common 100-pin 0.65mm-pitch QFP Foot Pattern.

*To purchase the IC61-TOOL-4 pull-out tool which detaches an MCU on IC61 Series, please contact Yamaichi Elect Co., LTD.





©2005 Renesas Technology Corp., All Rights Reserved.