Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on May 22, 2006: RSO-R0E521000EPB00_2-060522D

The Converter Board R0E521276CFG00
for the R8C/26 and R8C/27 Groups of
MCUs Released

We have released the converter board--R0E521276CFG00--for connecting the emulation probe R0E521000EPB00* or the compact emulator R0E521000CPE00 to any MCU of the R8C/26 and R8C/27 groups in the user system, which is encapsulated in the 32-pin 0.8-mm-pitch LQFP.

* for the PC7501 emulator

  1. Features
    The R0E521276CFG00 converter board connects the R0E521000EPB00 emulation probe or the R0E521000CPE00 compact emulator to any MCU of the R8C/26 and R8C/27 groups in the user system, which is encapsulated in the 32-pin 0.8-mm-pitch LQFP (PLQP0032GB-A), and enables you to emulate the MCU.
    For the specifications of the R0E521276CFG00, see the user's manual.

    To emulate MCUs of the R8C/26 and R8C/27 groups, it is necessary to use the MCU files that contain the information specific to the MCUs.

    MCU file is included in a latest emulator debugger. (Updated Jul. 5, 2007)
    Please download an update program from the following and update to the latest emulator debugger.

    Download latest release notes from the following. You can also get them by using the DocumantUpdater.



    NOTICE:
    In each of the release note are described the notices that must be taken when you debug and evaluate programs written for MCUs of the R8C/26, R8C/27, R8C/28, and R8C/29 groups. So be sure to read through it before using the emulation probe and the compact emulator.

    And, for detailed information on the R0E521000EPB00 emulation probe and the R0E521000CPE00 compact emulator, visit the Web sites below.
    - R0E521000EPB00 Datasheets
    - R0E521000CPE00 Datasheets


  2. The Contents of the Product Package
    (1)   A converter board--R0E521276CFG00--for the R8C/26 and R8C/27 groups
    (2)   A joint connector for ICE--YQPACK032SA (manufactured by Tokyo Eletech Corp.)
    (3)   A target board connector--NQPACK032SA (manufactured by Tokyo Eletech Corp.)
    (4)   Four guide pins--YQ-GUIDE (manufactured by Tokyo Eletech Corp.)
    (5)   A user's manual


  3. Ordering Information
    If you place an order for the product, please supply the following items of information to your local Renesas Technology sales office or distributor:

    3.1   R0E521276CFG00 Board Only
    Product type: R0E521276CFG00
    Type name: R0E521276CFG00

    3.2   Combinations of the Board and the R0E521000EPB00; and the R0E521000CPE00
    The sets of the R0E521276CFG00 board and the R0E521000EPB00 emulation probe; and the R0E521000CPE00 compact emulator are available.
    (1)   The set of the R0E521276CFG00 board and the R0E521000EPB00 probe: R0E521276EPB00
    Product type R0E521276EPB00
    Type name R0E521276EPB00

    (2)   The set of the R0E521276CFG00 board and the R0E521000CPE00 compact emulator: R0E521276CPE00
    Product type R0E521276CPE00
    Type name R0E521276CPE00

    For the prices of the above, contact your local Renesas Technology sales office or distributor.





© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal