Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on August 1, 2006: 060801/tn10

Hardware Tools Released
in the Last Half of July 2006


We released the hardware tools described below in the last half of July 2006.



  1. The E200F Emulator R0E0200F2EMU00
    (For the SH7785 group, SH7780 series, SuperH RISC engine family)
    As tracing capability improved, this emulator enables you to acquire trace information at 600-MHz operation. For details go to the datasheet.

    NOTICE:
    This emulator must be used in combination with the E200F emulator software V.1.06 Release 00 or later. For details of it, see RENESAS TOOL NEWS Doc. NO. 060801/tn6, "The E200F Emulator Software Revised to V.1.06 Release 00" published on August 1, 2006.


  2. Debugging MCU Boards for the SH/Tiny Series, SuperH RISC Engine Family
    (1)   HS7124EDB01H
    (For the SH7124 MCU group, encapsulated in the PLQP0048JA-A
    [previous FP-48F] package)
    (2)   HS7125EDB01H
    (For the SH7125 MCU group encapsulated in the PLQP0064KB-A
    [previous FP-64K] package)
    (3)   HS7125EDB02H
    (For the SH7125 MCU group encapsulated in the PRQP0064GB-A
    [previous FP-64A] package)

    By using each of these boards together with the E10A-USB on-chip debugging emulator HS0005KCU02H, the emulator operates as a simplified in-circuit emulator. So debugging capabilities such as performance measurement and tracing can be utilized, and among the pins of any SH/Tiny MCU, all those shared with H-UDI can be assigned to the user's functions.
    For details of the boards, see the datasheet.

    The sets of each board and the E10A-USB emulator HS0005KCU02H are available. Their product types are as follows:
    (1)   HS7124EDB01H-E1: set of HS7124EDB01H and E10A-USB
    (2)   HS7125EDB01H-E1: set of HS7125EDB01H and E10A-USB
    (3)   HS7125EDB02H-E1: set of HS7125EDB02H and E10A-USB


  3. Ordering Information
    • The E200F emulator for the SH7785 group
      Product Type Type Name
      R0E0200F2EMU00 as left

    • The debugging MCU boards for the SH/Tiny series
      Product Type Type Name
      HS7124EDB01H as left
      HS7125EDB01H as left
      HS7125EDB02H as left

    • The sets of each of the above boards and the E10A-USB emulator HS0005KCU02H
      Product Type Type Name
      HS7124EDB01H-E1 as left
      HS7125EDB01H-E1 as left
      HS7125EDB02H-E1 as left

© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal