|
|
 |
RENESAS TOOL NEWS on September 16, 2006: 060916/tn13
| Hardware Tools Released
in the First Half of September 2006 |
We released the hardware tools listed below in the first half of this September.
- For the M16C/Tiny Series, M16C Family
| (1) |
|
The M3028BT-EPB emulation probe for the PC7501 emulator
For details see its data sheets.
|
| (2) |
|
The M30280T-85LGF converter board
This converter board is used to connects any member of M16C/28 group of MCUs encapsulated in the PTLG0085JB-A package (85-pin 0.65-mm-pitch TFLGA) to the M3028BT-EPB emulation probe or the M30290T2-CPE compact emulator (both used for the M16C/Tiny series). The board can also be used for the previous product M30290T-EPB.
For details of the converter board, see its User's Manual (pdf).
|
| (3) |
|
Combinations of the M3028BT-EPB emulation probe and a converter board
| Product Type |
Emulation Probe and Converter Board |
| M3028BT-EPB-1 |
M3028BT-EPB and M30263T-42SSB |
| M3028BT-EPB-2 |
M3028BT-EPB and M30260T-48FPD |
| M3028BT-EPB-3 |
M3028BT-EPB and M30291T-64FPD |
| M3028BT-EPB-4 |
M3028BT-EPB and M30290T-80FPD |
| M3028BT-EPB-5 |
M3028BT-EPB and M30280T-85LGF |
|
- Ordering Information
The product types for ordering the above products are as follows
(the type names are the same as the product types):
| Product Type |
| M3028BT-EPB |
| M30280T-85LGF |
| M3028BT-EPB-1 |
| M3028BT-EPB-2 |
| M3028BT-EPB-3 |
| M3028BT-EPB-4 |
| M3028BT-EPB-5 |
|
|
 |