|
|
 |
RENESAS TOOL NEWS on October 1, 2006: 061001/tn4
| The Debuggers for the M32R MCU Family Revised |
The debuggers for the M32R MCU family have been revised to the following:
- The emulator debugger M3T-PD32RM V.3.01 Release 00
(for the M32100T5-SDI-E, M32100T3-SDI-E, and M32100T-EZ-E emulators)
- The emulator debugger M3T-PD32R V.5.01 Release 00
(for the M32100T2-SDI-E emulator; and the M32120T-SDI, M32100T-SDI-E, M32170T-SDI, M32310T-SDI-E, and M32310T-SDI emulators for spare and repair)
- The simulator debugger M3T-PD32RSIM V.3.01 Release 00
(included with the C/C++ compiler package--M3T-CC32R--for the M32R family)
- Descriptions of Revision
| 1.1 |
|
To the M3T-PD32RM and M3T-PD32R emulator debuggers, the following four MCU files have been introduced:
32185.mcu, 32186.mcu, 32195.mcu, and 32196.mcu
These are used for the 32185, 32186, 32195, and 32196 MCU groups respectively.
|
| 1.2 |
|
The following problems have been fixed:
| (1) |
|
With saving a mixed representation of source and disassembled code on a text file
For details, see RENESAS TOOL NEWS published on June 16, 2006
|
| (2) |
|
With referencing member variables of a structure, union, or class
For details, see RENESAS TOOL NEWS published on January 16, 2006
|
| (3) |
|
An error arises when the MCU receives the reset signal from the target system during the period from setting execution of a target program to starting the execution (the M3T-PD32RM only)
This problem has been resolved by prohibiting the debugger from receiving the reset signal. |
|
- How to Update Yours
Free-of-charge online update is available. So download the update program of the product you want to update from the Web sites at
M3T-PD32RM
M3T-PD32R
M3T-PD32RSIM
|
 |