|
|
 |
RENESAS TOOL NEWS on November 1, 2006: 061101/tn7
|
Corrections to a Catalog
Published in October 2006 |
We notify corrections to the catalog "Renesas Quick Reference Guide to
Semiconductor Devices, Document No. REJ02A0003-0700" (published in October
2006).
These corrections will be seen on HERE from December 2006 on.
- Corrections to Renesas Quick Reference Guide to Semiconductor Devices,
Document No. REJ02A0003-0700 (published in October 2006):
- Page 89, body of the table; third from the bottom in the Emulator
column (third from the right)
Remove *6 in PC7501 *6
- Ibid.; second from the bottom in the Emulator column (third from the
right)
Remove *6 in PC7501 *6
- Page 96, under the table, last of the notes
Add the following note:
*** Under planning
- Page 99, title name of the table
Read Operating Environment for R8C/Tiny Series
for Operating Environment for M16C/Tiny Series
- Page 106, body of the table; top in the Low-cost model Emulator column
(second from the left)
Make a cell for the H8/38447 and H8/38427 groups only and
put (E8) R0E000080KCE00 in it.
- Page 107, body of the table; fourth from the top in the Emulator MCU
or Emulator MCU board column (fourth from the left)
Read M38267RLFS or M37560RLFS *11 for M38267RLFS
- Ibid., under the table; last of the numbered list
Add the following note:
| |
*11. |
|
The M38267RLFS does not have the 10-bit A/D conversion
mode function. Use M37560RLFS for the software development
of 10-bit A/D. The M37560RLFS can be used also for the DTMF
function and the CTCSS function of the 3826A group. |
- Related Information
We notified corrections to this catalog in the following RENESAS TOOL NEWS.
|
 |