Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on December 15, 2006: 061215/tn1

A Note on Using
the E8 Emulator Software V.2.09 Release 00


Please take note of the following problem in using the emulator software for the E8 on-chip debugging emulator:
  • With using the R8C/Tiny E8 emulator debugger


1. Product and Version Concerned
   The E8 emulator software V.2.09 Release 00

2. Description
   When user programs are downloaded to target MCUs using the R8C/Tiny E8 
   emulator debugger, which is included in the product, "Communication Timeout 
   Errors" may arise.

3. Conditions
   This problem arises if the following conditions are all satisfied:
    (1) The R8C/Tiny E8 emulator debugger V.2.05.00, which is included in 
        the product concerned is used.

        To see the version number of your emulator debugger, perform the 
        following steps:
         (a) In the High-performance Embedded Workshop, open the Tool menu 
             and select the Administration command. The Administration 
             dialog box appears, showing you the Registered Components 
             list box.
         (b) Read the version number of the component "R8C E8 SYSTEM" in 
             the Debugger Components folder, which is displayed in the 
             above list box. The version number of the product concerned 
             is "2.05.00".

   (2) Any of the following MCUs in the R8C/Tiny series is targeted:
       - R5F21206, R5F21207, and R5F21208 MCUs; R8C/20 group
       - R5F21216, R5F21217, and R5F21218 MCUs; R8C/21 group
       - R5F21226, R5F21227, and R5F21228 MCUs; R8C/22 group
       - R5F21236, R5F21237, and R5F21238 MCUs; R8C/23 group
       - R5F21244, R5F21245, R5F21246, R5F21247, and R5F21248 MCUs;
            R8C/24 group
       - R5F21254, R5F21255, R5F21256, R5F21257, and R5F21258 MCUs;
            R8C/25 group
       - R5F21262, R5F21264, R5F21265, and R5F21266 MCUs; R8C/26 group
       - R5F21272, R5F21274, R5F21275, and R5F21276 MCUs; R8C/27 group
       - R5F21282 and R5F21284 MCUs; R8C/28 group
       - R5F21292 and R5F21294 MCUs; R8C/29 group

   (3) The E8 emulator is connected to the PC using a hub based on 
       USB 2.0 standards. Depending on PCs, the problem may occurs 
       if no hub is used.

4. Workarounds
   When you are using a hub based on USB 2.0 standards, remove the hub 
   to connect the E8 directly to the PC.
   If the problem is still not resolved, replace your emulator software 
   with the previous version, V.2.08 Release 00.

5. Schedule of Fixing the Problem
   We are releasing the problem-fixed version of the product before long.


© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal