Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on December 16, 2006: 061216/tn1

The AutoUpdate Utility Revised to V.1.02.00


We have revised the AutoUpdate utility from V.1.01.00 to V.1.02.00.


1. Descriptions of Revision
1.1 Functions Introduced and Improved
    (1) Improved are items and contents in several dialog boxes displayed 
        when the AutoUpdate wizard is stepped through.
    (2) In the Configure AutoUpdate dialog box, the method of downloading 
        application programs can be chosen between "Renesas Tools Web Site" 
        and "Local or Network Drive."

1.2 Problems and Errors Corrected
    The following problems and errors have been corrected:
    (1) In the Select Applications dialog box, the list of applications 
        to be updated and the characters displayed at the bottom of the 
        dialog box are overlaid in some cases.
    (2) In the function for displaying update information on the system 
        tray, update information on applications not to be updated is 
        provided.
    (3) Contents of the help for each button in the Select Applications 
        dialog box and the Select Updates dialog box.

2. How to Update Your Utility
   Update yours using your AutoUpdate utility itself. The update service 
   will be available on and after December 20.
   You are also able to update yours by downloading the update program 
   from the downloa site.



© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal