|
|
 |
RENESAS TOOL NEWS on December 16, 2006: 061216/tn5
| The C Compiler Package--M3T-NC308WA--
for the M32C MCU Series
Revised to V.5.41 Release 01 |
We have revised the C compiler package--M3T-NC308WA--for the M32C series*
from V.5.41 Release 00 to V.5.41 Release 01.
* The M32C series is the generic name of the M32C/90, M32C/80, and M16C/80
series of MCUs.
1. Description of Revision
The problem "With automatic generation of variable interrupt- and special
page vector tables," which was notified in RENESAS TOOL NEWS Document No. 061016/tn1, has been fixed.
2. How to Update Your Product and Purchase the Revised One
2.1 Free-of-Charge Update
Free-of-charge online update is available. If you are using the product
concerned, download the installer of the update program
from the download site and execute it.
2.2 First Ordering
If you place an order for the product, please supply the following
items of information to your local Renesas Technology sales office
or distributor (for the price of the product, also contact them):
Product Type: The C compiler package for the M32C series
Version No.: V.5.41
Release No.: Release 01
Host OS: Windows XP, Windows Me, Windows 98, Windows 2000,
or Windows NT 4.0
|
 |