Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on December 21, 2006: 061221/tn1

A Note on Uninstalling
the Flash Development Toolkit
V.3.06 Release 00 and V.3.07 Release 00


Please take note of the problem stated below with uninstalling the Flash Development Toolkit V.3.06 Release 00 and V.3.07 Release 00. (These toolkits are used for programming flash memory in the SuperH RISC engine, M16C, H8SX, H8S, H8, and 740 families of MCUs.)


1. Description
   If you uninstall the Flash Development Toolkit V.3.06 Release 00 or 
   V.3.07 Release00 through the Add/Remove Programs dialog box in Windows' 
   Control Panel, the information of registered software tools for the 
   AutoUpdate Utility may also be removed. 
   If this is the case, the AutoUpdate Utility will not operate properly. 
   In this case, please re-install all your products supporting 
   AutoUpdate Utility.
   Even if you have updated your toolkit from V.3.06 Release 00 or 
   V.3.07 Release 00 to V.3.07 Release 01, this problem will also 
   arise. However, if you have installed V.3.07 Release 01, this 
   problem will be eliminated.

2. Workaround
   We have provided the uninstaller of the Flash Development Toolkit V.3.06 
   and V.3.07. Please visit here to see detail.
   


© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal