|
|
 |
RENESAS TOOL NEWS on February 16, 2007: 070216/tn6
| Converter Boards for the R8C/2A, R8C/2B, R8C/2C,
and R8C/2D MCU Groups Released |
We have released three converter boards* for the R8C/2A, R8C/2B, R8C/2C,
and R8C/2D MCU groups.
*Used together with the emulation probe--R0E521000EPB00--or the compact
emulator--R0E521000CPE00--for the R8C/Tiny MCU series.
1. Outlines
Three converter boards for the R8C/2A, R8C/2B, R8C/2C, and R8C/2D groups
connect the R0E521000EPB00 emulation probe or the R0E521000CPE00 compact
emulator with target MCUs of the R8C/2A, R8C/2B, R8C/2C, or R8C/2D
group to emulate them.
The product types of these converter boards are listed below.
For details of the specifications of the boards, see the user's manuals
of them. The Web pages shown below will be opened from February 20 on.
(1) The converter board for connecting the 64-pin 0.8-mm-pitch LQFP
package (PLQP0064GA-A) of the R8C/2A and R8C/2B groups:
R0E5212BACFG00
The user's manual (230K bytes in PDF)
(2) The converter board for connecting the 64-pin 0.5-mm-pitch LQFP
package (PLQP0064KB-A) of the R8C/2A and R8C/2B groups:
R0E5212BACFK00
The user's manual (249K bytes in PDF)
(3) The converter board for connecting the 80-pin 0.5-mm-pitch LQFP
package (PLQP0080KB-A) of the R8C/2C and R8C/2D groups:
R0E5212DACFK00
The user's manual (221K bytes in PDF)
For general descriptions of the R0E521000EPB00 emulation probe and the
R0E521000CPE00 compact emulator, see their datasheets on the Web sites
for the emulation probe, and this page for the compact emulator.
To emulate any MCU of the R8C/2A, R8C/2B, R8C/2C, and R8C/2D groups,
you need a firmware file and an MCU files (containing information
specific to the MCU).
MCU file is included in a latest emulator debugger. (Updated Jul. 5, 2007)
Please download an update program from the following and update to the latest emulator debugger.
- M16C R8C PC7501 emulator debugger
http://www.renesas.com/pc7501_download
- M16C R8C compact emulator debugger
http://www.renesas.com/m16c_cpe_dbg_download
Download latest release notes from the following. You can also get them by using the DocumantUpdater.
R0E521000EPB00 Release Notes
R0E521000CPE00 Release Notes
Note:
In each release note are described important notes on debugging and
evaluating the MCUs of the R8C/2A, R8C/2B, R8C/2C, and R8C/2D groups.
So please read it carefully before using the emulation probe and the
compact emulator.
2. Contents of Product Packages
2.1 R0E5212BACFG00
(1) A converter board--R0E5212BACFG00--for connecting the 64-pin
0.8-mm-pitch LQFP package (PLQP0064GA-A) of the R8C/2A and
R8C/2B groups
(2) A socket at a probe end--YQPACK064SA (manufactured by Tokyo
Eletech Corp.)
(3) A socket for mounting the target MCU--NQPACK064SA160
(manufactured by Tokyo Eletech Corp.)
(4) Four guide pins--YQ-GUIDE (manufactured by Tokyo Eletech Corp.)
(5) A user's manual
2.2 R0E5212BACFK00
(1) A converter board--R0E5212BACFK00--for connecting the 64-pin
0.5-mm-pitch LQFP package (PLQP0064KB-A) of the R8C/2A and
R8C/2B groups
(2) A socket at a probe end--YQPACK064SD (manufactured by Tokyo
Eletech Corp.)
(3) A socket for mounting the target MCU--NQPACK064SD-ND
(manufactured by Tokyo Eletech Corp.)
(4) Four guide pins--YQ-GUIDE (manufactured by Tokyo Eletech Corp.)
(5) A user's manual
2.3 R0E5212DACFK00
(1) A converter board--R0E5212DACFK00--for connecting the 80-pin
0.5-mm-pitch LQFP package (PLQP0080KB-A) of the R8C/2C and
R8C/2D groups
(2) A socket at a probe end--YQPACK080SD (manufactured by Tokyo
Eletech Corp.)
(3) A socket for mounting the target MCU--NQPACK080SD-ND
(manufactured by Tokyo Eletech Corp.)
(4) Four guide pins--YQ-GUIDE (manufactured by Tokyo Eletech Corp.)
(5) A user's manual
3. Ordering Information
If you place an order for any of the converter boards, please supply
the following items of information to your local Renesas Technology
sales office or distributor (for the prices of the product, also
contact them):
3.1 Converter Board Only
Product Types Type Names
-----------------------------
R0E5212BACFG00 As left
R0E5212BACFK00 As left
R0E5212DACFK00 As left
3.2 Combination of Converter Board and Emulation Probe/Compact Emulator
to Be Released on March 1
Each of the three converter boards can be supplied in combination
with the R0E521000EPB00 emulation probe or the R0E521000CPE00
compact emulator.
3.2.1 R0E5212BACFG00 Board with Emulation Probe/Compact Emulator
to be released on March 1
(1) The combination with the emulation probe
Product Type: R0E5212BAEPB00
Type Name: As above
(2) The combination with the compact emulator
Product Type: R0E5212BACPE00
Type Name: As above
3.2.2 R0E5212BACFK00 Board with Emulation Probe/Compact Emulator
to be released on March 1
(1) The combination with the emulation probe
Product Type: R0E5212BAEPB10
Type Name: As above
(2) The combination with the compact emulator
Product Type: R0E5212BACPE10
Type Name: As above
3.2.3 R0E5212DACFK00 Board with Emulation Probe/Compact Emulator
to be released on March 1
(1) The combination with the emulation probe
Product Type: R0E5212DAEPB00
Type Name: As above
(2) The combination with the compact emulator
Product Type: R0E5212DACPE00
Type Name: As above
|
 |