Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on March 16, 2007: 070316/tn2

A Note on Using the High-performance Embedded Workshop V.4.02.00
--With Moving Workspaces--


Please take note of the following problem in using the High-performance Embedded Workshop V.4.02.00:
  • With moving workspaces


1. Description
   If you move a workspace from the working directory to another and open 
   the workspace, a blank dialog box (a Warning dialog box) may appear; 
   if you close this dialog box, you will unable to open the workspace. 
   In such a case, usually the following message will be dispatched:
    --------------------
    Warning

    This workspace has been moved.
    Old directory: xxxxxxxxxx
    New directory: xxxxxxxxxx
    Do you want to continue opening this workspace?
    Yes        No        Cancel
    --------------------

2. Condition
   This problem occurs if you use the High-performance Embedded Workshop 
   V.4.02.00 on the secondary monitor of a multi-monitoring system.

3. Workarounds
   This problem can be avoided in either of the following ways:
   (1) Use the High-performance Embedded Workshop V.4.02.00 on 
       the primary monitor.
   (2) If you want to use the High-performance Embedded Workshop V.4.02.00 
       on the secondary monitor, change the settings of the Options by going
       through the following steps before opening 
       the workspace that has been moved:
       (a) Open the Setup menu and select the Options command 
           to open the Options dialog box.
       (b) Click the Confirmation tab in the Options  dialog box.
       (c) Uncheck the Open a moved workspace check box in the 
           Options dialog box.
       (d) Click the OK button in the Options dialog box.
       After changing the settings of the Options, 
       you are able to open workspaces without displaying the Warning dialog 
       box.

4. Schedule of Fixing the Problem
   We plan to fix this problem in the next release of the product.



© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal