Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on July 1, 2007: 070701/tn9

Notes on Using Flash Development Toolkit


Please take note of the problems described below in using Flash Development Toolkit. (This toolkit is used for writing programs into flash memories in the SuperH RISC engine, M16C, H8SX, H8S, H8, and 740 families of MCUs.)

1. Product and Versions Concerned
   Flash Development Toolkit V.3.05 through V.3.07

2. Descriptions
   If the user system is equipped with the COM1 port and any COM1* ports 
   other than COM1 (for example, COM10, COM11, COM100, and so on; "*" means 
   the wild-card), COM1 cannot be selected in the "Select port" drop-down 
   list in the Communication Port dialog because COM1 is not provided in 
   the list.
   And if the user system is equipped with the COM2 port and any COM2* 
   ports other than COM2 (for example, COM20, COM21, COM200, and so on; "*" 
   means the wild-card), COM2 cannot be selected in the "Select port" 
   drop-down list in the Communication Port dialog because COM2 is not 
   provided in the list.

3. Workaround
   Delete COM1* and COM2*.



© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal