|
|
 |
RENESAS TOOL NEWS on August 1, 2007: 070801/tn11
| Flash Development Toolkit Revised to V.3.07 Release 03 |
We have revised Flash Development Toolkit from V.3.07 Release 02 to
V.3.07 Release 03. (This toolkit is used for the SuperH RISC engine, M16C,
H8SX, H8S, H8, and 740 families of MCUs to program on-chip flash memory.)
1. Descriptions of Revision
1.1 Supported MCUs Increased
The following MCUs have been added to the support line:
(1) In the H8 family (3 MCUs)
H8/38776F, H8/38704F, and H8/38702F
(2) In the M16C family (26 MCUs)
Group MCUs
---------------------------------------------------------
M16C/30P M3030SFEP, M3030SFDP, M3030RFGP, M3030RFEP
M3030RFDP, M3030RFCP, M3030RFAP, M30304GEP
M30304GDP, and M30302GGP
R8C/2D R5F212DC and R5F212DA
R8C/2C R5F212CC and R5F212CA
R8C/2B R5F212BC and R5F212BA
R8C/2A R5F212AC and R5F212AA
R8C/23 R5F2123C and R5F2123A
R8C/22 R5F2122C and R5F2122A
R8C/21 R5F2121C and R5F2121A
R8C/20 R5F2120C and R5F2120A
Note that the flash memory in the above MCUs can be programmed
only via the E8 emulator.
(3) In 740 family
Group MCU
---------------------------------------------------------
38D5 M38D59FF
The flash memory in this MCU can also be programmed only via the E8.
1.2 A Problem with the Firmware for the E8 Emulator Resolved
Resolved has been the problem with the firmware for the E8 that
signals may conflict with each other in the E8 when flash memory in
the 740 family is programmed using the toolkit and the E8.
NOTICE:
If you use any of the versions of the toolkit shown in (1) below with
the E8 for a long time to program flash memory in any of the MCUs
listed in (2), programming will be performed correctly, but the E8
may suffer a breakdown. So in such a case use Flash Development
Toolkit V.3.07 Release 03 or later.
(1) Versions Concerned
Flash Development Toolkit V.3.05 Release 00 through
V.3.07 Release 02 and V.4.00 Release 00
(2) MCUs Involved
Group MCUs
------------------------------------------------------
7516 M37516F4 and M37516F8
38D5 M38D59FF
3851 M38517F8
3850A M38507F8A
3804L M38049FFL
3804H M38049FFH
3803L M38039FFL
3803H M38039FFH
2. How to Update Your Product
Free-of-charge online update is available. Download the installer of
the latest version of the toolkit from the Web site at
http://www.renesas.com/fdt_download
and execute it. This site will be opened from August 6 on.
Note that you are not able to update your toolkit to V.3.07 Release 03
using AutoUpdate Utility.
3. Notices
(1) This revision is not the one from Flash Development Toolkit V.4.00
Release 00, but for making V.3 capable of supporting the MCUs added
to the support line in V.4.00 Release 00.
(2) If you execute AutoUpdate Utility in the PC where Flash Development
Toolkit V.3.07 Release 03 has been installed, the evaluation version
of Toolkit V.4 will be installed.
Attention:
Change in Download Function and Product Information Pages
Since June 1st, 2007, download data and product information
have only been updated on the Renesas global web site
(http://www.renesas.com/homepage.jsp), not our regional web sites.
For the latest versions of download data and product information,
please visit our global web site.
This is a temporary situation and regional web sites will be updated
once again by the end of August.
Technical documentation and Tool News newsletter are not effected
by this temporary situation and you can still find the latest support
information on both our regional and global web sites.
Thank you for your understanding.
|
 |