|
|
 |
RENESAS TOOL NEWS on September 1, 2007: 070901/tn1
| A Note on Using AutoUpdate Utility |
Please take note of the following problem in using AutoUpdate Utility:
- With updating the C/C++ compiler packages for the SuperH family, and
the H8SX, H8S, and H8 families of MCUs
1. Description
Even when you have updated a compiler package using AutoUpdate Utility,
the Updater of the compiler package may be detected by the utility.
2. Conditions
This problem occurs in both the following cases:
(1) The C/C++ compiler package for the SuperH family has been updated
from V.9.01 Release 00 to V.9.01 Release 01 using AutoUpdate
Utility.
(2) The C/C++ compiler package for the H8SX, H8S, and H8 families has
been updated from V.6.01 Release 03 to V.6.02 Release 00 using
AutoUpdate Utility.
3. Workaround
If you encounter this problem, perform the following procedure to change
the settings of AutoUpdate Utility:
(1) Invoke AutoUpdate Utility. The "Welcome to AutoUpdate Wizard"
window opens.
(2) Click the Next button. The window for selecting applications
appears.
(3) Uncheck the check boxes for the following products to be updated
in the Applications list:
(1) Application name:
C/C++ compiler package for SuperH RISC engine family
Version No.: 9.01.00
(2) Application name:
C/C++ compiler package for the H8, H8S, and H8SX
Version No.: 6.01.03
(4) Click the Next button. The search window for updating information
appears.
(5) Click Next to open The Finished window.
(6) Click the Finish button.
4. Schedule of Fixing the Problem
We plan to fix this problem in the next release of both products.
|
 |