|
|
 |
RENESAS TOOL NEWS on September 5, 2007: 070905/tn1
| The C/C++ Compiler Package for the H8SX, H8S, and H8
MCU Families
Revised to V.6.02 Release 00 |
We have revised the C/C++ compiler package for the H8SX, H8S, and H8 MCU
families from V.6.01 Release 03 to V.6.02 Release 00.
1. Descriptions of Revision
1.1 High-performance Embedded Workshop Updated
The High-performance Embedded Workshop included in the package has been
updated to V.4.03.00. For details of this version, see RENESAS TOOL NEWS
Document No. 070701/tn3, published on July 1, 2007, at
http://tool-support.renesas.com/eng/toolnews/070701/tn3.htm
1.2 Functions Introduced in the Compiler
(1) Option divs_inst introduced: It expands division expressions to
division instructions without using shift operations and is used
for MCUs capable of executing division instructions at high
speed of the H8SX family.
(2) Option align=4 can be used for the H8S MCU family.
(3) Reduced has been the object sizes of mathematical functions
sinf(), cosf(), tanf(), expf(), logf(), sqrtf(), and atanf(),
which handle single-precision floating-point numbers, in order
to improve speed and precision in operations.
1.3 Functions Introduced in the Optimizing Linkage Editor
The following options have been introduced in the optimizing
linkage editor (hereafter abbreviated as the linker):
(1) total_size: Outputs the total size of sections to the standard
output type by type of section listed below.
- Executable section
- ROM-allocated data section
- RAM-allocated data section
(2) show=total_size: Outputs the above total size of sections to
the linkage list.
1.4 Problems Fixed
1.4.1 In High-performance Embedded Workshop
The problem reported in the following item of news has been fixed:
(1) RENESAS TOOL NEWS Document No. 070701/tn2, published on
July 1, 2007, at
http://tool-support.renesas.com/eng/toolnews/070701/tn2.htm
1.4.2 In the Compiler
The following problems have been fixed:
(1) Those reported in the following items of news:
(a) RENESAS TOOL NEWS Document No. RSO-H8C_2-060601D, published
on June 1, 2006, at
http://tool-support.renesas.com/eng/toolnews/060601/tn6.htm
(b) RENESAS TOOL NEWS Document No. 070901/tn4, published
on September 1, 2007, at
http://tool-support.renesas.com/eng/toolnews/070901/tn4.htm
(2) The problem that option cpu=300L or cpu=300 cannot be selected
with option structreg at the same time
(3) The problem that the results of execution of standard library
functions sscanf() and realloc() are incorrect
(4) The problems that may cause the C4980, C332, C3027, C4633,
and C4979 errors to arise
(5) The problem that the debugger may reference incorrect members of
a structure and union.
1.4.3 In the Linker
(1) For the message numbers L0300, L1330, L2220, and L3110,
the method of displaying messages has bee improved as follows:
If the file causing to dispatch a message of these types is
a specific library module in the library files, the library
module's name can be provided in the linker V.9.03.00 or later.
Example of a message before improved (V.9.02.00 or earlier)
** L3110 (F) Illegal cpu type "<CPU type>" in "<library name>"
Example of a message after improved (V.9.03.00 or later)
** L3110 (F) Illegal cpu type "<CPU type>" in "<library name>
(<module name>)"
To check for the version number of your linker, use the
following procedure:
(a) In High-performance Embedded Workshop, open the Tools menu
and select Administration. The Tool Administration dialog
box appears.
(b) Select the compiler package you are using among Toolchains
in the Registered Components list of the above dialog box;
then click the Properties button. The Properties dialog box
opens.
(c) In the Information tab of this dialog box, the version
numbers of your tools will be shown.
Example of a linker: Optimizing Linkage Editor (V.9.00.02)
(2) Fixed has been the problem that Call Walker, the stack analyzing
tool, provides a smaller value of the program's stack usage
than the actual one.
This problem may occur if the following conditions are all
satisfied:
(a) Optimizing option -optimize=1 is selected at compilation.
(b) In the C source file exists a function calling another
one that immediately follows it.
Example of C source file:
-----------------------------------------
void f()
{
. . . . . . . . . . . . . . . . . . . .
g(); /* Function f calls g, which follows f */
}
void g()
{
. . . . . . . . . . . . . . . . . . . .
}
-----------------------------------------
(3) Fixed has been the problem that the register to be saved and
that to be restored are different from each other when an option
enabling the optimization of saving and restoring registers
(for example, optimize=register) is used.
This problem may occur if the following conditions are all
satisfied:
(a) Option "goptimize" is selected at compilation.
(b) Any of the following CPU options is selected at compilation:
300, 300reg, 300hn, 300ha, 2000n, 2000a, 2600n, and 2600a
Note that 2000n, 2000a, 2600n, and 2600a are involved if
each of them is used together with compiler option legacy=v4.
(c) The version of your linker is V.9.00.01 or later.
(d) Any option enabling the optimization of saving and restoring
registers (for example, optimize=register) is used at linking.
(4) The problems causing the following internal errors have been fixed:
- L4000 (-) Internal Error : (1153)
- L4000 (-) Internal Error : (3081)
- L4000 (-) Internal Error : (8870)
- L4000 (-) Internal Error : (8957)
2. How to Update Your Product and Purchase the Revised One
2.1 Free-of-Charge Update
Free-of-charge online update is available. Update yours using
AutoUpdate Utility or download the update program from the Web site
at
http://www.renesas.com/h8c_download
and execute it (this site will be opened from September 5 on).
2.2 First Ordering
If you place an order for the product, please supply the following
items of information to your local Renesas Technology sales office
or distributor:
Product Type: The C/C++ compiler package for the H8SX, H8S, and
H8 MCU families
Version No.: V.6.02
Release No.: Release 00
Host OS: Windows XP or Windows 2000
For the price of the product, also contact the above.
3. Notice when using the MISRA C Rule Checker SQMlint
V.1.02 Release 00 through V.1.03 Release 00
Refer to RENESAS TOOL NEWS Document No. 070901/tn2, published on
September 3, 2007, if you are using the MISRA C Rule Checker SQMlint
V.1.02 Release 00 through V.1.03 Release 00
http://tool-support.renesas.com/eng/toolnews/070901/tn2.htm.
|
 |