1. Features
(1) The products conform to the uITRON 4.0 specifications.
(2) GUI introduced to the configurator, which allows you easily to make
initial settings of application programs on M3T-MR100K/4 and S/4.
(3) The products support the same functionality as M3T-MR308K/4 and S/4
(these are used for the M32C/80, M16C/80, and M16C/70 MCU series).
So application programs containing M3T-MR308K/4 or S/4 can be ported
to those using M3T-MR100K/4 and S/4 without difficulty.
For details of the specifications of the products, see their datasheets
on the Web site at
http://www.renesas.com/m3t_mr100_4
(this site will be opened from October 4 on)
2. How to Purchase the Products
When you place an order for M3T-MR100K/4 or S/4, please supply
the following items of information to your local Renesas Technology
sales office or distributor:
| Product Type: |
M3T-MR100K/4 (evaluation license) or
M3T-MR100S/4 (mass-production license) |
| Type Name: |
R0R56400TRW01wE |
NOTICE:
Letter w denotes the types of license. It shall be replaced with
any one of the following numerals or letters:
1: |
Evaluation license; a real-time OS can be installed only
to one host computer. |
5: |
Evaluation license; a real-time OS can be installed
up to 5 host computers. |
A: |
Evaluation license; a real-time OS can be installed
up to 10 host computers. |
K: |
Mass-production license; a real-time OS can be embedded up to
a total of 1,000 productions of product model(s) with the source
code not disclosed. |
U: |
Mass-production license; a real-time OS can be embedded up to
unlimited productions of product model(s) with the source code
not disclosed. |
Z: |
Mass-production license; a real-time OS can be embedded up to
unlimited productions of product model(s) with the source code
disclosed. |
Example:
For mass-production license up to a total of 1,000 productions for
any MCU of the R32C/100 series with the source code not disclosed,
the type name is R0R56400TRW01KE.