Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on October 1, 2007: 071001/tn5

The Emulator Software Products
for two E200F Emulators Revised
to V.1.08 Release 00


We have revised the emulator software products for the E200F emulators R0E0200F0EMU00* and R0E0200F2EMU00** from V.1.07 Release 01 to V.1.08 Release 00. These emulators and software products emulate systems designed with SH-4A and SH4AL-DSP CPU-cored MCUs in the SuperH RISC engine family.

*for SH-Mobile.
**for SH7780 series.

1. Products to Be Updated
    - Emulator software V.1.00 Release 00 through V.1.07 Release 01*
        for the E200F emulator R0E0200F0EMU00
    - Emulator software V.1.06 Release 00 through V.1.07 Release 01*
        for the E200F emulator R0E0200F2EMU00

   *We have not informed you of the revision of V.1.07 Release 00 to 
    V.1.07 Release 01. The latter is different from the former only in that 
    the latter's self-diagnostic program has been revised from V.1.1.02 
    to V.1.1.03.

2. Description of Revision
   The following device group can be supported by the R0E0200F2EMU00 
   emulator:
MCU Series Device Group
SH7780 SH7722(SH-MobileR)
3. How to Update Yours
   Free-of-charge online update is scheduled on October 10.
   Use AutoUpdate Utility on and after October 10.
   Otherwise, use the following procedure:
(1) Download the update program (a ZIP file) of the product you want from the Web site at http://www.renesas.com/e200f_download This site will be opened from October 4 on. (2) Decompress the downloaded ZIP file to obtain the installer program HewInstMan.exe and execute it. 4. Notice If the installer program is executed in the system where High-performance Embedded Workshop V.4.02.00 or earlier resides, it will be upgraded to V.4.03.00.

© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal