Tool News
 
 
 

Tool News

Products Info
Downloads
Tools FAQs
RENESAS TOOL NEWS on November 1, 2007: 071101/tn3

The Beta Software of the Cycle-Accurate Simulator Debugger for the M16C/60, /30, /20, /10, /Tiny, and R8C/Tiny MCU Series Released


The beta software of the M16C R8C cycle-accurate simulator debugger has been released. The distribution of this beta software aims to be subjected to users' evaluation in the accuracy of cycle measurement, ease of operation, and so on so that the specifications of the commercial product can be refined.
We will much appreciate your advice sent by e-mail to us at
http://www.renesas.com/inquiry

1. Outline
   The M16C R8C cycle-accurate simulator debugger is a simulator debugger 
   in which the accuracy of cycle count measurement has much been improved 
   than in the existing M16C R8C simulator debugger.

2. Extended Capabilities
   The software enables you to measure cycle counts in consideration of 
   bus width, instruction-queue buffers, and the number of wait states.
   The extended capabilities newly introduced are as follows:
   (1) To make settings of bus width and the number of access cycles 
       to memory.
   (2) To simulate operations of instruction-queue buffers and busses.
   (3) To improve the accuracy of cycle counts in Bus mode in the Trace 
       window.

3. How to Get and Install the Beta Software
   Download the installer of the software from the below download file 
   and execute it. The Web page will be opened from November 6 on.
   Download File:M16CCASim_V010R00Beta.exe
   File size: 77.2MB

   NOTICE:
     The installer of the beta software overwrites the M16C R8C simulator 
     debugger. So, if you have already installed the M16C R8C simulator 
     debugger, install the beta software into another directory.
     For further information, see the release note of the beta software 
     on the Web page at
http://documentation.renesas.com/eng/products/tool/rej10j1749_m16ccasimsw_n.pdf



© 2008. Renesas Technology Corp., All rights reserved. Privacy | Legal